FB#.RESREFPHASE

Description

This parameter sets the electrical degrees of phase lag in the resolver.

See the motor resolver datasheet for the value for this parameter.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

electrical degrees

Range

-180 to 180°

Default Value

-2°

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.RESREFPHASE

3500h

05h

Signed32

-

1000:1

Read/Write

No

FB2.RESREFPHASE

3501h

05h

Signed32

-

1000:1

Read/Write

No

FB3.RESREFPHASE

3502h

05h

Signed32

-

1000:1

Read/Write

No

FB4.RESREFPHASE

3503h

05h

Signed32

-

1000:1

Read/Write

No

FB5.RESREFPHASE

3504h

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30160

1

30160 (0x75d0)

FB1.RESREFPHASE

Signed32

Read/Write

Yes

30161

1

30161 (0x75d1)

FB2.RESREFPHASE

Signed32

Read/Write

Yes

30162

1

30162 (0x75d2)

FB3.RESREFPHASE

Signed32

Read/Write

Yes

30163

1

30163 (0x75d3)

FB4.RESREFPHASE

Signed32

Read/Write

Yes

30164

1

30164 (0x75d4)

FB5.RESREFPHASE

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.RESREFPHASE

30160

Float

Read/Write

-

FB2.RESREFPHASE

30161

Float

Read/Write

-

FB3.RESREFPHASE

30162

Float

Read/Write

-

FB4.RESREFPHASE

30163

Float

Read/Write

-

FB5.RESREFPHASE

30164

Float

Read/Write

-